Key Interlock Systems
Interlocks help protect against unauthorized operation Factory installed only on heavy duty safety switches from 30 A to 1200 A, Type 12 and 304 stainless steel Type 4X. Not available on hazardous location devices (Type 7/9) or fiberglass reinforced polyester (Type 4X).
The key interlock system is a simple and easy method of applying individual key interlock units and assemblies to the above equipment so as to require operation in a predetermined sequence.
Quoting: Contact Schneider Electric for catalog number, availability, and pricing prior to quoting a job. Detailed information is required before an order can be processed.
Ordering: Order cannot be released for production until the following information has been provided:
-
End User–Company name, address.
-
Function of each lock (e.g., switch to be locked open with key removed, key held when switch is closed).
-
Existing Equipment–if switch is to be interlocked with equipment already on site, provide brand of existing lock and key number.
-
Other New Equipment–if switch is to be interlocked with new equipment not yet installed at the site, then provide contact person and phone number so that locks may be coordinated.
-
Additional information may be required upon order entry.
Use these suffixes on switch catalog numbers:
-
KI = 1 lock per switch
-
KI2 = 1 lock with 2 cylinders (2 keys) per switch
-
KIKI = 2 separate locks per switch