80210–100–12

Validity Note

This instruction bulletin is valid for Square D NEMA 2 Rated Gasket Cover Kits in the North American region only.

For product compliance with environmental directives such as RoHS, REACH, PEP, and EOLI, go to www.se.com/green-premium.

For technical characteristics of the physical modules described in this bulletin, go to www.se.com.

The technical characteristics presented in this bulletin should be the same as those that appear online. We may revise content over time to improve clarity and accuracy. If you see a difference between the information contained in this bulletin and online information, use the online information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?