Secure Disposal Guidelines

Secure disposal refers to systematically retiring outdated legacy software and hardware without compromising business needs or compliance requirements. Disposal is defined as the act of discarding media with no other sanitization considerations. Examples of disposal include deleting electronic documents using standard file deletion methods, discarding paper in a recycling container, and discarding electronic storage media in a standard trash receptacle.

iOS and Android Devices

For secure disposal on iOS or Android, follow the device’s standard way of removing an app.

Windows Devices

If the Windows app is configured to use Shared Data, you need to remove the shared data if you are no longer going to use that device for Mobile XI.

In the event that you remove shared data when one user uninstalls the app yet other users are still using the app on that device, the shared data is removed for all users and they'll have to download the shared data again.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?