ArcFM XI Series Solution Center

The Solution Center is a comprehensive app for managing your ArcFM XI tenants. You can:

  • Manage users

  • Configure markups

  • Create Session Manager sessions

  • Configure operational maps, reference maps, and basemaps to be used in your applications

  • Monitor services and incidents

  • Configure autoupdaters, dynamic workflows, and client-side workflows

  • Manage offline replicas and tile packages


The ArcFM Solution Center Implementation Guide is available on the Documentation Portal and provides invaluable information, such as:


ACE Tool

The ArcFM Connectivity Evaluator {ACE} tool is a separate application from Solution Center, and its core function is to test and verify connectivity to ArcFM services and, depending on the application, connectivity to Azure Service Bus.


Client Configuration

In the Client Configuration plugin you can configure tenant level settings such as portal logins, root certificates, and hybrid connections. This is a crucial prerequisite prior to performing Solution Center configuration or any XI series app configuration, given that you need connectivity for the configuration to work.


User Management

As ArcFM plugins are added, such as Designer XI and Editor XI, licenses are recorded in Solution Center where they can be monitored. Based on which plugins are added, the User Management plugin provides a tab near the top for each product, allowing you to track the number of user licenses accessed over specific time periods.

The Esri license model for ArcGIS Pro varies by both level and type. See the ArcGIS Pro licensing article for more information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?