Add and Edit Resources
In asset management, a resource group is a collection of logically grouped items. They are organized by function that can influence intervention actions. Each one is configured with a unit cost and group name. Some examples of group names include OPEX, CAPEX, Sustainability, Inventory, and Contractors. This gives you the flexibility to use resources in different interventions to show the cost associated with each action.
To add a new resource:
-
From the upper right corner, click Add resource.
-
Enter the name of the resource.
-
Enter the unit cost for the group.
If the Is financial option is enabled, the unit value is 1.
-
Select the name of the group from the menu and click Add Resource.
New group names can be added if needed.
To edit an existing resource, click Edit, change the values, and
click Edit resource to update the value.
You can also use the groups as a filter. Select the group from the list and the assets in that resource group are listed. Select as many filters as needed.