Fiber Connectivity and Circuit Trace

Whether a fiber has a circuit or not, the trace procedure is the same.
  1. Locate the desired fiber optic cable, then click the Fibers tab.
  2. Scroll to locate the desired fiber.
    1. If a circuit is present, click the Circuit name to initiate the trace.

    2. If no circuit is present, click the name “none” to initiate the trace.

  3. The Details tab provides summary information of the trace:

  4. The Path tab provides a one-line diagram of the trace.

    TIP: On the Path tab, you can click the Flip  icon to reverse the start and end points of the one-line diagram.
  5. Click any cable or facility name along the path to see more information about that component.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?