Scenario and Program States
States are settings that you configure to communicate the status of each program and scenario built to show multi-year plans. They are listed in menus to help understand what state each program or scenario is at in the creation process.
Create a Program State
Program states focus on specific asset categories and use the metrics to model maintenance costs and monetized risk over time. To create a new program state:
-
Click Create program state.
-
In the window that opens, enter a title and enable the applicable settings. Then, at the bottom of the window, click Create program state.
These options are available.
-
Lock program prevents further program changes.
-
Lock recomputing prevents recalculation of asset’s algorithms.
-
Treat assets prevents an asset from use in another program.
-
Once the program state is created, the title and lock settings can be modified from the list.

Create a Scenario State
Scenario states focus on showing the scenario status and the publishing viability for each scenario. The state is mapped to a program state and color coded for easy reference.
To create a new scenario state: