Send Session
Available in: ArcFM (Process Tasks toolbar), ArcFM Viewer for ArcGIS Engine (Available Tasks), Session Manager (Available Tasks)
Enable:
-
Select session in Session Manager
-
Open session in ArcFM or ArcFM Viewer for ArcGIS Engine (edit or redline session)
The Send Session task allows you to send a session regardless of whether you're sending it from the enterprise or the field. This task is available in the Available Tasks lists in the applications listed above and as a button on the Session Manager toolbar in ArcFM Viewer for ArcGIS Engine.
- Select a session in Session Manager or open a session in ArcFM or ArcFM Viewer for ArcGIS Engine.
- Select the Send Session task in the Available tasks list
and click the green Execute button. If you have the session open in
ArcFM Viewer for ArcGIS Engine, you may select the Send Session
button on the Session Manager toolbar.
- On the Select New Owner screen, select a recipient for
the session and click OK.
When this task is executed, it determines whether the user is in the field or on the enterprise. For field users, it presents a list of enterprise users. The field user selects a recipient of the session and clicks OK. The session packet is then sent to that user on the enterprise.
The opposite is true when the task is executed on the enterprise. The user is presented with a list of field users. The enterprise user selects a field editor and clicks OK. The session packet is then mobilized and sent to the selected field editor.