Change Owner to Include All Users
Changes the owner of a design to another user.
Enabled
-
The node passed to this subtask must be a design or work request.
-
At least one user must exist in the MM_PX_USER table.
Execute
-
Identifies the users with the appropriate roles assigned to own the selected node.
-
Allows the user to select from a list of valid users.
-
Assigns the node to the chosen user.
Parameters
-
DefaultUser: takes a user name as a value.
-
AutoChangeOwner: takes a value of 0 or 1. 0=False, prompt the user to select owner; 1=True, select default owner without prompt.