Inspector
The Inspector extension is available only in ArcFM Viewer for ArcGIS Engine. It allows the user to edit non-spatial attributes, and create, update, and delete related objects in the field. This implementation also includes the ability to place redline graphics (either as simple graphics or as annotation). The Inspector tool makes it easy for mobile users to perform inspections (e.g., pole inspections) and manage related objects.
Required Licenses in the Field: Inspector Extension and ArcFM Viewer for ArcGIS Engine
Field Databases: Backdrop, Login (optional), Session Manager
Perform the following steps to configure Inspector.
STEP 1: Set Up Directory Structure
Geodatabase Replication Directory Permissions
Update Replication Service Login
STEP 2: Configure Graphic Annotation
Optional. Perform this configuration if you wish to store graphics in an annotation layer.
STEP 3: Create Backdrop Database
Create/Import Graphic Favorites Optional. Do this step ONLY if you do not have a Login database.
OPTIONAL: Create Login Database
The Login database is necessary only if you wish to provide the field user with user/system favorites. If you aren't using favorites, there's no need for the Login database. If you have no login database, graphic favorites can be imported into the Backdrop.
Create/Import Graphic Favorites
STEP 4: Create Session Manager Databases
Configure Enterprise Process Framework Database
Configure Field Process Framework Database