Mobile ArcFM
Mobile ArcFM provides all the functionality of the enterprise while in the field. The mobile user has full editing capabilities, and can create or delete features while in the field.
Required Licenses in the Field: ArcFM
Field Databases: Backdrop, Login (optional), Session Manager
Perform the following steps to configure Mobile ArcFM in the field.
STEP 1: Set Up Directory Structure
Geodatabase Replication Directory Permissions
Update Replication Service Login
STEP 2: Configure Graphic Annotation
Optional. Perform this configuration if you wish to store graphics in an annotation layer.
STEP 3: Create Backdrop Geodatabase
Perform the optional configurations below ONLY if you do not have a Login database. The Backdrop Replica step is necessary.
Create/Import Graphic Favorites (optional)
Import Feature Favorites (optional)
OPTIONAL: Create Login Database
The Login database is necessary only if you wish to provide the field user with user/system favorites. If you aren't using favorites, there's no need for the Login database. If you have no login database, graphic favorites can be imported into the Backdrop.
Create or Import Graphic Favorites
STEP 4: Create Session Manager Database
Configure Enterprise Process Framework Database
Configure Field Process Framework Database