Mobile Designer
Mobile Designer provides the mobile user with Designer functionality while in the field. The user can receive, create and edit designs, then send them to the enterprise.
Required Licenses in the Field: Designer
Field Databases: Backdrop, Workflow Manager
Perform the following steps to configure Designer in the field.
STEP 1: Set Up Directory Structure
Geodatabase Replication Directory Permissions
Update Replication Service Login
STEP 2: Configure Graphic Annotation
Optional. Perform this configuration if you wish to store graphics in an annotation layer.
STEP 3: Create Backdrop Database
Create/Import Graphic Favorites
STEP 4: Create Workflow Manager Databases
Configure Enterprise Process Framework Database
Configure Field Process Framework Database