Set Up Directory Structure
Mobile and Geodatabase Replication require a specific directory structure that allows Mobile packets to be transferred between the field and enterprise. Before starting your configuration for Mobile or Geodatabase Replication, create the directories as indicated below. This ensures you have the directories needed for storing the necessary databases created in the configuration process.
If you're setting up multiple field machines, the directory structure must be the same on all of them. You can create the structure on one administrator machine, then disseminate the same information to all field machines.
-
Machine 1: Enterprise - This machine has ArcFM/Designer installed. It may also host the Geodatabase Replication server.
-
Machine 2: Administrator - This machine has ArcFM/Designer installed and the exact same directory structure as all field machines. Use the configuration files and directory structures on this machine to deploy to all field machines.
-
Machines 3-x: Field - These are the machines used in the field and will have only ArcFM Viewer or ArcFM Viewer for ArcGIS Engine and any necessary Mobile extensions (e.g., Inspector, Redliner).
Mobile Directory Structure - with Geodatabase Replication
This directory structure is necessary if you're planning to use Geodatabase Replication to maintain an updated backdrop database in the field as well as send/receive sessions and designs. If you elect to create a login database, Geodatabase Replication will also ensure login databases in the field are synchronized with the login database on the Enterprise.
The image below illustrates set up on the Administrator machine. Once configuration is complete, copy the directory structure on the Administrator machine (along with the databases highlighted in green in the Field Directory Structure) to all field machines.

Server (Enterprise):
Create the following directories on the server or Enterprise machine. These directories do not have to be named exactly as shown.
-
ReplicationServer: This is the Server Base Directory used by Geodatabase Replication to send/receive sessions and designs. It also uses this directory to maintain the backdrop database and the login database.
-
InitialExtract: This directory contains all initial extract databases for all replicas. For Mobile, this will be one or more backdrop replicas. You can break the backdrop into regions (e.g., Northwest, Southeast). This results in multiple backdrop databases (one for each region) and multiple backdrop replicas (one for each database).
-
ProcessFramework: This directory must be created by an administrator on the Enterprise machine and be available for all client machines to access. It provides the necessary directory structure to transport Mobile sessions and designs between the field and Enterprise. Make note of the path to this directory. In a later step, you'll create a configuration value (ProcessFrameworkEnterprise value) in the Process Framework database that points to this directory. All other folders shown in this directory are created automatically during the initial send/receive. No files in the ProcessFrameworkServer directory should ever be edited manually.
-
Login: This directory stores the optional login database. Use a directory replica to distribute this database to field machines and update it in the field, should the Enterprise version change. If you choose not to use a login database (recommended), then you will not need this directory.
TIP: Note that the login database is optional. Schneider Electric recommends adding the necessary stored display and graphic favorites to the Backdrop database to eliminate the need for a Login database.
Once you have the directory structure set up on the server (Enterprise) machine, you will need to assign permissions to the ReplicationServer and ProcessFramework directories.
Administrator Machine (Field Machines):
Create the following directories on the Administrator machine. When setup is complete, copy this directory structure (and the backdrop and Process Framework databases) to all field machines. The paths on the Administrator machine and the field machines must be EXACTLY the same.
-
ReplicationField: This is the Client Base Directory used by Geodatabase Replication to send/receive sessions and designs. It also uses this directory to maintain the backdrop database and the login database.
-
Backdrop: This directory must have the same name as the replica for your backdrop database. If you have multiple backdrop databases and replicas, then you will have multiple backdrop directories. These directories will be named for the replicas (e.g., Northwest, Southeast). Each replica will hold the initial extract database. Before copying these directories/databases to field machines, open each database in ArcMap and ensure the stored display layers are properly connected.
-
ProcessFramework: This is the directory where Mobile sessions and designs are transported between the field and Enterprise. Make note of the path to this directory. In a later step, you'll create a configuration value (ProcessFrameworkField value) in the Process Framework database that points to this directory. If you do not create this directory and the configuration value, then Mobile will automatically use this location instead: C:\Documents and Settings\<username>\Application Data\Miner and Miner\ProcessFrameworkField. All other folders shown in this directory are created automatically during the initial send/receive. This directory must be readable and writable. This directory may hold your field Process Framework Database, but it doesn't have to. You can place this database in another location.
-
Login: A directory replica will place the login database in this location (if it's been properly configured). If you choose not to use a login database (recommended), then you will not need this directory.
Directories on the field machines require no special sharing or permissions.
Mobile Directory Structure - No Geodatabase Replication
Server (Enterprise):
Create the following directory on the server or Enterprise machine. This directory does not have to be named exactly as shown.
-
ProcessFramework: This directory must be created by an administrator on the Enterprise machine and be available for all client machines to access. It provides the necessary directory structure to transport Mobile sessions and designs between the field and Enterprise. Make note of the path to this directory. In a later step, you'll create a configuration value (ProcessFrameworkEnterprise value) in the Process Framework database that points to this directory. All other folders shown in this directory are created automatically during the initial send/receive. No files in the ProcessFrameworkServer directory should ever be edited manually.
Once you have the directory structure set up on the server (Enterprise) machine, you will need to assign permissions to the ProcessFramework directory.
Administrator Machine (Field Machines):
Create the following directory on the Administrator machine. When setup is complete, copy this directory structure (and the Process Framework databases) to all field machines. The paths on the Administrator machine and the field machines must be EXACTLY the same.
-
ProcessFramework: This is the directory where Mobile sessions and designs are transported between the field and Enterprise. Make note of the path to this directory. In a later step, you'll create a configuration value (ProcessFrameworkField value) in the Process Framework database that points to this directory. If you do not create this directory and the configuration value, then Mobile will automatically use this location instead: C:\Documents and Settings\<username>\Application Data\Miner and Miner\ProcessFrameworkField. All other folders shown in this directory are created automatically during the initial send/receive. This directory must be readable and writable. This directory may hold your field Process Framework Database, but it doesn't have to. You can place this database in another location.
Directories on the field machines require no special sharing or permissions.
Directory Permissions
This step is necessary for all Mobile users, regardless of whether you're using Geodatabase Replication.
Ensure that any Windows users who will be accessing Mobile have the necessary permissions to create and delete files on the enterprise Process Framework directory (e.g., ProcessFrameworkServer) and its subdirectories.
- On the Enterprise machine, Browse to the Mobile directory (e.g., ReplicationServer, ProcessFrameworkServer).
- Right-click the directory and select Properties.
- Select the Security tab.
- If the Everyone group exists in the list, select it and click Edit. Skip to step 8.
- Click Add. Windows 7: Click Edit, then click Add.
- Type Everyone in the "Enter the object names to select" field and click OK.
- Select the Everyone group and select the checkboxes for all permissions available except Special Permissions. You may also create a separate group including only Mobile users or assign permissions individually. Click OK.
- Click the Advanced button to display the Advanced Security Settings.
- Ensure the Apply To field for the Everyone group indicates "This folder, subfolders and files." If it doesn't, select the row and click Change Permissions, and then click Edit.
- From the Apply To field, select "This folder, subfolders and files."
- Click OK to dismiss the Permission Entry window.
- Click OK to dismiss the Advanced Security Settings window.
- Click OK to dismiss the Properties window.
GDBR Directory Permissions
This step is necessary only if you're using Geodatabase Replication.
The domain user created in the Before You Begin section must be used to run the Geodatabase Replication Server Service. This domain user must have permissions on the server base path to modify and delete any files created by a user who previously ran replication. Follow the instructions below to assign the proper permissions.
- On the Geodatabase Replication server, browse to the server base path (e.g., ReplicationServer, ServerBase) created in the Before You Begin section. Right-click the server base path directory and select Properties.
- Select the Security tab and click Add to add the domain user. Windows 7: Click Edit, then click Add.
- On the Select Users, Computers, or Groups window, click Advanced.
- Ensure the From This Location field contains the domain in which the user resides. Click Find Now to list all users.
- Browse to the domain user created in the Before You Begin section. Select it and click OK.
- Click OK on the Select Users, Computers, or Groups window.
- On the Security tab, ensure the domain user is selected
and assign the following permissions by selecting the checkboxes in
the Permissions window.
-
Modify
-
Read & Execute
-
List Folder Contents
-
Read
-
Write
-
- Click OK to save changes.
The remaining permissions (Full Control and Special Permissions) are not required. However, assigning additional permissions will not cause Geodatabase Replication to fail.
Next, update the login user for the Geodatabase Replication service on the server machine.
Update Replication Service Login
This step is necessary only if you are using Geodatabase Replication.
The domain user created in the Before You Begin section is used to run the Geodatabase Replication Server Service. This step gives the domain user access to log in to the service.
- On the replication server, open Computer Management.
- Expand Services and Applications.
- Select Services.
- In the right-side pane, right-click ArcFM Geodatabase Replication Service and select Properties.
- Select the Log On tab.
- In the This Account fields, type the domain user and password.
- Click OK.