Submit Design
Changes the design’s status to Pending Approval and allows the user to assign it to an approval officer.
Enabled
-
MMWorkflowManager must be the current extension.
-
The selected node is a design node.
-
There may not be another approved design in the same work request. If there is another approved design, the subtask is disabled.
Execute
-
Prompts the user to select an approval officer.
-
Attempts to transfer ownership.
-
Tells the builder that the user has changed so it can update the tree if necessary.
-
If ownership is changed, the design is closed.