Fiber Colors
Fiber Manager supports several methods of color-coding buffer tubes and fiber strands. As fiber technology has improved, more and more fibers are inserted into buffer tubes, and the traditional twelve-color method is no longer adequate to track individual fiber strands in high-count cables.. Fiber Manager supports stripes (up to 3), blocks (up to 3), and color combinations to fully represent fiber strand hierarchies.
Color Coding Method |
Representation in the Color Domain |
---|---|
Solid Color |
In the database domain, type a single integer value representing the color along with a user-friendly description. |
One Stripe |
To add a stripe, immediately after the solid color integer, type a dash followed by the integer value for the stripe color. For example, a black stripe is -0, a white stripe is -16777215, a red stripe is -16711680, etc. Also type a user-friendly description. |
Two Stripes |
To add two stripes, immediately after the first stripe color integer, type another dash and integer value for the second stripe color. For example, two black stripes is -0-0, a black stripe and a red stripe is -0-16711680, etc. Also type a user-friendly description. |
One Block |
To add a block, immediately after the solid color integer, type a dash followed by the letter “B” and the integer value for the block color. For example, a black block is -B0, a white block is -B16777215, a red block is -B16711680, etc. Also type a user-friendly description. |
Two Blocks |
To add two blocks, immediately after the first block color integer, type another dash followed by the letter “B” and the integer value for the block color. For example, two black blocks is -B0-B0, a black block and a red block is -B0-B16711680, etc. Also type a user-friendly description. |
Stripes and Blocks |
You can combine colors, stripes, and blocks by combining the methods above. For example, two black stripes and 2 black blocks is -0-0-B0-B0, two black stripes and 2 red blocks is -0-0-B16711680-B16711680, etc. Also type a user-friendly description. |
Color choices are seen throughout the application.
-
In Connection Manager:
-
In Fiber Manager Reports:
-
In Fiber Manager dialogs. In particular, notice in the following image that the user-friendly description helps clarify the block patterns on these buffer tubes:
Properties:
-
Field Type: Text
-
Domain Type: Coded Values
-
Split Policy: Duplicate
-
Merge Policy: Default Value
Coded Values:
Code |
Description |
---|---|
Solid Color |
|
255 |
Blue |
16744448 |
Orange |
65280 |
Green |
8404992 |
Brown |
12632256 |
Slate |
16777215 |
White |
16711680 |
Red |
0 |
Black |
16776960 |
Yellow |
16711935 |
Violet |
16754856 |
Rose |
655355 |
Aqua |
Solid Color with 1 Stripe |
|
255-0 |
Blue - 1 Stripe |
16744448-0 |
Orange - 1 Stripe |
65280-0 |
Green - 1 Stripe |
8404992-0 |
Brown - 1 Stripe |
12632256-0 |
Slate - 1 Stripe |
16777215-0 |
White - 1 Stripe |
16711680-0 |
Red - 1 Stripe |
0-16777215 |
Black - 1 Stripe |
16776960-0 |
Yellow - 1 Stripe |
16711935-0 |
Violet - 1 Stripe |
16754856-0 |
Rose - 1 Stripe |
655355-0 |
Aqua - 1 Stripe |
Solid Color with 2 Stripes |
|
255-0-0 |
Blue - 2 Stripes |
16744448-0-0 |
Orange - 2 Stripes |
65280-0-0 |
Green - 2 Stripes |
8404992-0-0 |
Brown - 2 Stripes |
12632256-0-0 |
Slate - 2 Stripes |
16777215-0-0 |
White - 2 Stripes |
16711680-0-0 |
Red - 2 Stripes |
0-16777215-16777215 |
Black - 2 Stripes |
16776960-0-0 |
Yellow - 2 Stripes |
16711935-0-0 |
Violet - 2 Stripes |
16754856-0-0 |
Rose - 2 Stripes |
655355-0-0 |
Aqua - 2 Stripes |
Solid Color with 1 Black Block |
|
255-B0 |
Blue - 1 Black Block |
16744448-B0 |
Orange - 1 Black Block |
65280-B0 |
Green - 1 Black Block |
8404992-B0 |
Brown - 1 Black Block |
12632256-B0 |
Slate - 1 Black Block |
16777215-B0 |
White - 1 Black Block |
16711680-B0 |
Red - 1 Black Block |
0-B16777215 |
Black - 1 White Block |
16776960-B0 |
Yellow - 1 Black Block |
16711935-B0 |
Violet - 1 Black Block |
16754856-B0 |
Rose - 1 Black Block |
655355-B0 |
Aqua - 1 Black Block |
Solid Color with 2 Black Blocks |
|
255-B0-B0 |
Blue - 2 Black Blocks |
16744448-B0-B0 |
Orange - 2 Black Blocks |
65280-B0-B0 |
Green - 2 Black Blocks |
etc. |
etc. |
Solid Color with 3 Black Blocks |
|
255-B0-B0-B0 |
Blue - 3 Black Blocks |
16744448-B0-B0-B0 |
Orange - 3 Black Blocks |
65280-B0-B0-B0 |
Green - 3 Black Blocks |
etc. |
etc. |
Solid Color with 1 Stripe and 1 Black Block |
|
255-0-B0 |
Blue - 1 Stripe - 1 Black Block |
16744448-0-B0 |
Orange - 1 Stripe - 1 Black Block |
65280-0-B0 |
Green - 1 Stripe - 1 Black Block |
etc. |
etc. |
Solid Color with 1 Stripe and 1 Red Block |
|
255-0-B16711680 |
Blue - 1 Stripe - 1 Red Block |
16744448-0-B16711680 |
Orange - 1 Stripe - 1 Red Block |
65280-0-B16711680 |
Green - 1 Stripe - 1 Red Block |
etc. |
etc. |
Solid Color with 2 Stripes, 1 Black Block, 1 Red Block |
|
255-0-0-B0-B16711680 |
Blue - 2 Stripes - 1 Black Block - 1 Red Block |
16744448-0-0-B0-B16711680 |
Orange - 2 Stripes - 1 Black Block - 1 Red Block |
65280-0-0-B0-B16711680 |
Green - 2 Stripes - 1 Black Block - 1 Red Block |
etc. |
etc. |