ArcFM Options

There are several options listed in the ArcFM Options under the ArcMap Customize menu.

  • The General options tab allows you to determine the Zoom To scale, the size of the flash for the Highlight tool, and other options.

  • The Attribute Editor options tab allows you to modify various Attribute Editor options.

  • The Editing options tab allows you to modify various editing functions.

  • The Map Production options tab allows you to designate a default path for an exported map file.

  • The Phase Swap options tab allows you to determine how phase swap traces are performed.

QR code for this page

Was this helpful?