Available Tasks Tool

Available in: ArcFM (Process Tasks toolbar), ArcFM Viewer for ArcGIS Engine, Session Manager, Workflow Manager

Enable: Open a session or design in ArcFM or ArcFM Viewer. In Session Manager and Workflow Manager, this tool is always enabled.

The Task tool offers an easy method for performing actions in your Process Framework extension. When you select a node, the Available Tasks tool drop-down menu shows the actions that may be performed on that node. Simply select a node, choose a task from the menu, and click the Execute Task button.

Available tasks in Session Manager:


ArcFM Process Tasks toolbar in ArcFM:

The ArcFM Process Tasks toolbar is not available in ArcFM Viewer for ArcGIS Engine. The Available Tasks tool appears on the Session Manager toolbar instead.

Available tasks on the Session Manager toolbar in ArcFM Viewer for ArcGIS Engine:

The current install includes sample subtasks for Session Manager and Workflow Manager. Your administrator may also create and edit Tasks using the Process Framework Administration tool (see the online help for the Admin tool). Descriptions of the sample subtasks provided are available in the Set Up Process Framework Tools section of the Configuring ArcFM Solution online help in ArcCatalog.

QR code for this page

Was this helpful?