Designer Express Toolbar
The Designer Express toolbar provides the following tools.
Opens Workflow Manager, the only place you can create or open express designs. |
|
![]() Save Express Design |
Saves the edits made to the open express design. NOTE: If you end the edit session you will not be able to save your express design or changes to it. |
![]() |
Closes the express design after reconciling and posting it. |
![]() |
Displays the Design Estimate window. This window calculates an estimated cost of the express design. |
Lists all available palettes. Select a palette to display its design features in the Design Palette tab. |
|
![]() |
Opens the Palette Manager. Use the Palette Manager to create, edit and delete palettes. |
![]() |
This tool marks a feature (or group of features) as abandoned. However, the feature will not be actually abandoned until after the express design is converted. |
![]() |
This tool marks a feature (or group of features) as abandoned and removed. However, the feature will not be actually abandoned and removed until after the express design is converted to a standard design. |
![]() |
This tool allows you to select a regular feature, create a corresponding design feature class (DFC) based on the selected feature. |
![]() |
This tool copies design feature classes (DFCs) and their associated cost items from other express designs into the open express design. |
![]() |
This tool show or hide express designs. It also allows you to copy whole express designs. |
This tool provides the ability to add, edit or delete the cost items. |