Settings for Features with Color
These settings apply to any feature or object classes.
Any feature or object in the fiber data set can use color. For example, the F_FIBER and F_BUFFERTUBE tables use color to identify strands and the tubes containing them.
-
The Example Field Name, Data Type, and Domain columns contain values entered while creating the feature. If using the worksheet, record these values in Table 5.
-
The Assign Field Model Name column contains a value entered in the ArcFM Properties Manager dialog, Field Model Names tab. If using the worksheet, record these values in Table 5.
Function |
Settings |
|||
---|---|---|---|---|
Example Field |
Data Type |
Domain |
Assign Field Model Name |
|
Features that have color |
FiberColoredField |
Text |
Fiber Colors |
FIBERCOLOREDFIELD |
FiberColorNameField |
Text |
Fiber Color Names |
FIBERCOLORNAMEFIELD |