Approve Imported Design
Approves a design on the enterprise after it has been approved in the field and imported into the enterprise database.
Enabled
-
MMWorkflowManager must be the current extension.
-
The node passed to this subtask must be a design.
Execute
-
Checks to see if the design has been approved and skips the design if it has not been approved.
-
If any design in the same work request has already been approved, it will be unapproved.
-
Approves the imported design on the enterprise.
-
Checks the MM_PX_CONFIG table to see if the ConstructOnApprove flag has been set. If it is set, the Work Request is assigned the state of In Construction.