Assign ArcFMGDBReplicationService Directory Permissions
This step must be performed if you're doing a distributed implementation. The domain user’s group must have permissions to the ArcFMGDBReplicationBase directory and to C:\Windows\Temp. The ArcFMGDBReplicationService directory is created when ArcFM Geodatabase Replication Web is installed.
- In Windows Explorer, browse to the ArcFMGDBReplicationService directory (C:\Inetpub\wwwroot\ArcFMGDBReplicationService by default).
- Right-click ArcFMGDBReplicationService and select Properties.
- On the Security tab click Edit.
- This displays the Permissions window. Click Add.
- Add the IIS_WPG or IIS_IUSRS user group (e.g., domain\IIS_WPG or domain\IIS_IUSRS).
- Assign the user or group the following permissions: Read & Execute, List Folder Contents, Read. Optionally: Write, Modify.
- Click OK.
- Perform these steps again to assign the same permissions for the same user/group to the C:\Windows\Temp directory.