Feeder Manager 1.0 Configuration Steps

Step 1: Create domains

Step 2: Identify the feature classes to include in the network

Step 3: Set sources

Step 4: Add model names to domain

Step 5: Configure CircuitSource object class

Step 6: Assign model names and field model names

Step 7: Export XML

Step 8: Initialize electric trace weights

Step 9: Build the geometric network

Step 10: Convert to ArcFM Objects

Step 11: Assign autoupdaters

Step 12: Configure default junctions

Step 13: Initialize FeederID Fields

Step 14: Add a Circuit to the Network

QR code for this page

Was this helpful?