Create Login Database

The Login database is necessary only if you wish to provide the field user with user/system favorites. If you aren't using favorites, there's no need for the Login database. If you have no login database, graphic favorites can be imported into the Backdrop.

QR code for this page

Was this helpful?