ArcFM Viewer for ArcGIS Engine

Engine Mobile provides all the functionality of the enterprise while in the field. The mobile user has full editing capabilities, and can create or delete features while in the field.

Required Licenses in the Field: ArcFM

Field Databases: Backdrop, Login (optional), Session Manager

Perform the following steps to configure Engine Mobile in the field.

STEP 1: Set Up Directory Structure

Mobile Directory Permissions

Geodatabase Replication Directory Permissions

Update Replication Service Login 

STEP 2: Configure Graphic Annotation

Optional. Perform this configuration if you wish to store graphics in an annotation layer. 

STEP 3: Create Backdrop Geodatabase

Perform the optional configurations below ONLY if you do not have a Login database. The Backdrop Replica step is necessary.

Create/Import Graphic Favorites (optional)

Import Feature Favorites (optional)

OPTIONAL: Create Login Database

The Login database is necessary only if you wish to provide the field user with user/system favorites. If you aren't using favorites, there's no need for the Login database. If you have no login database, graphic favorites can be imported into the Backdrop.

Create or Import Graphic Favorites

Import Feature Favorites

STEP 4: Create Session Manager Database

Configure Enterprise Process Framework Database

Configure Field Process Framework Database

STEP 5: Create Replicas

STEP 6: Set Up Mobile Synchronizer

Using Mobile Synchronizer

STEP 7: Deploy to Multiple Client Machines

QR code for this page

Was this helpful?