Engine Mobile Directory Structure without Geodatabase Replication

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

This directory structure is necessary if you're planning to use Mobile Synchronizer to send/receive sessions and designs and do not plan to use Geodatabase Replication to maintain the backdrop database in the field.

QR code for this page

Was this helpful?