Session Manager Database Connectivity

When the Session Manager application starts, the user will be prompted to log in to the database using OLEDB.


OLEDB Providers

The database client software, whether it is Oracle, SQL Server, or PostgreSQL, supplies a provider component that facilitates the client connection to the database server. The provider requires certain information in order to create a connection to the database. The user must specify the server to which he or she wants to connect. The server information required varies between Access, Oracle, Microsoft SQL Server, and PostgreSQL.

QR code for this page

Was this helpful?