Underground Facility Manager

Underground Facility Manager (UFM) allows you to create, view and manage underground facilities. This tool displays detailed diagrams of the facilities contained within a manhole. The Underground Facility Manager displays the duct banks as well as the individual ducts, their relationships to one another and conduit associations to the ducts.

Before configuring UFM, perform the basic Conduit Manager configuration.

  • STEP 1: Add Model Names

  • STEP 2: Create Domain

  • STEP 3: Create Classes

  • STEP 4: Create Relationships

  • STEP 5: Assign Model Names and AUs

  • STEP 6: Set Geodatabase Properties

  • STEP 7: Export XML

  • STEP 8: Create Map Document

IMPORTANT: A unique value must exist in the UndergroundStructure field that has the FACILITYID field model name assigned. If this FacilityID value is not assigned, some Underground Facility Manager tools will not work.

QR code for this page

Was this helpful?