Cable Report

The Cable Report displays high-level information about a selected cable, including available and defective fiber counts. Further, it displays detailed information about all circuits that pass through the selected cable.

Because this is an HTML-based report, it can be opened in any web browser.

To run the report, follow these steps:

  1. Select a cable in ArcMap.
  2. In the ArcFM Attribute Editor > Selection tab, right-click the selected cable and choose Create Cable Report.
  3. The report opens in a web browser. Further, all Fiber Manager reports are saved in the default directory C:\Users\username\Documents\ArcFM Solution\Fiber Manager\Reports.
QR code for this page

Was this helpful?