One Device Part of Multiple Incidents
Responder allows for a device to be added to more than one incident. The device must be in a Normal state on any and all incidents that it's a part of at the time of addition to a new incident. For example, if a device is part of a Switching Order (SO) Incident, and it has been opened and then closed back to a Normal state, a tool such as Create Fault or Add Fault could be used to add a fault on this device on an entirely different incident.
-
Two SOs are open in the Switch Order Editor in two separate browser tabs.
-
Each SO contains a step that has the same device assigned.
-
Each SO is part of a different incident.