Utility Tools
ArcFM utility tools let you navigate large map documents quickly by finding, highlighting, and moving features to the Selection tab. Access ArcFM utility tools by right-clicking a feature in a tree on many of the ArcFM Viewer tabs (e.g., Selection, ArcFM Locator, Identify tool, etc.) and selecting an option. Utility tools shown in blue are the default action. The default is the first option and the action that occurs when you double-click the feature.

Right-click options include:
-
Add to Selection
-
Feeder Manager Translator
-
Highlight
-
Pan To
-
Remove
-
View Conduit Configuration
-
Zoom To