Abandon Autoupdaters
The following autoupdaters are used by the Abandon tool. They are assigned in the ArcFM Properties Manager on the Abandon Info tab in the On Abandon field.
Component |
Description |
Used by Feature Classes |
Model Names Used |
Other Requirements |
Product Compatibility |
---|---|---|---|---|---|
ArcFM Abandon Unrelate and Relate |
Unrelates the ConductorInfo table from the conductor before it is abandoned and re-relates it to the conductor after it has been abandoned. |
Abandoned conductors, ConductorInfo table |
MMABANDONRELATE |
Details about configuring this autoupdater are available on the Relate/Unrelate ConductorInfo Table page. Refer to this documentation if you wish to configure this AU. |
Desktop Server |
ArcFM Change AbandonIndicator field |
Changes the value of the Abandon Indicator field to Yes. Abandon Indicator field must have the field model name MMAbandonIndicator assigned. |
Abandoned feature classes |
MMABANDONINDICATOR (FMN) |
Details about configuring to use the AbandonIndicator field are available on the Indicator Field page. |
Desktop Server |