Extended Feeder Manager
Extended Feeder Manager uses the same framework as Feeder Manager 1.0 and extends the functionality to help a utility manager to identify distinct voltage levels within an electric network. Extended Feeder Manager allows the utility manager to define a set of intermediate feeder sources within electric circuits at points downstream of the ultimate power sources recognized by Feeder Manager.
-
Add a Circuit or Subsource in Extended Feeder Manager (ArcFM only)
IMPORTANT: Deleting Conductors: When deleting multiple conductors, select them and use the Delete tool on the Attribute Editor (right-click and select Delete). The Esri delete tools (Delete key on the keyboard or Edit > Delete) do not interact well with Feeder Manager and may cause corrupted data when deleting multiple conductors on multiple feeders.