Folders

The tree to the left of the Switch Order Library displays all of the switch orders and switch order templates available. You can organize them by using folders. With the proper roles and permissions, you can right-click a folder in the tree to access the following tools:

Delete: Right-click any folder in the tree and select Delete to delete it from the library. You are then prompted to confirm that you want to delete the selected folder and everything in it.

New: The new tool provides a pull-out menu that lists three options. You can create a new folder to further organize your switching order library. You can also create a new switch order or template.

Cut/Paste: Use these tools to move folders. You can cut a folder and paste it into another folder.

Rename: Select a folder, and then click the text to rename it. This is not a right-click tool, and it is not available on switching orders and templates.

QR code for this page

Was this helpful?