Access Event Logging

You can send event logs to Schneider Electric Support to help troubleshoot problems. Event logging is always enabled. To access event logs on the different Windows operating systems, refer to the following instructions.

  • For Windows 2000 or XP:
    1. On a Windows 2000 or XP machine, click Start > Settings > Control Panel > AdministrativeTools > Event Viewer.
    2. In the Event Viewer, select Application Log under the Event Viewer (Local) tree.
    3. Click Action > Save Log File As and save this file to your local machine.
    4. Zip this file and go to Schneider Electric Support for additional information.
  • For Windows NT:
    1. On a Windows NT machine, click Start > Programs > Administrative Tools (Common) > Event Viewer. Event log files are also stored at C:\WINNT\system32\config\AppEvent.Evt.
    2. In the Event Viewer, select the Log menu and then select the Application option.
    3. Go to Log\Save As and save this file to your local machine.
    4. Zip this file and go to Schneider Electric Support for additional information.
  • For Windows 10:
    1. On a Windows 10 machine, search for Event Viewer in the Start menu.
    2. In the Event Viewer, select the Log menu and then select the Applications and Services option.
    3. Under Actions, choose either Save All Events As or Save Selected Events and save this file to your local machine.
    4. Zip this file and go to Schneider Electric Support for additional information.
QR code for this page

Was this helpful?