Session Manager Toolbar in ArcFM

The Session Manager toolbar in ArcMap allows you to access Session Manager and perform various tasks with an edit session or a redline session opened.

The following tool does not appear on the Session Manager toolbar by default. It must be added using the Customize menu.

Available Tasks/Execute Task: Many tasks in this list are also available as buttons on the toolbar. Following are those that are tasks only:

  • Change Session Owner

  • Edit Session

  • Unlock Session

QR code for this page

Was this helpful?