Connected Dimmers
Wiser Micro Module Dimmer |
Enables convenient multi-way switching and dimming by connecting up to 10 compatible momentary push-button switches. NOTE: Momentary push buttons must be certified for use in 220-240V AC applications.
Use for non Iconic wall plates such as Saturn Zen.
|
|
Iconic Connected Dimmer — Zigbee default |
Controls the lighting level in a room, or automatically sets lighting to a desired level in response to a specified condition or event using the push button. Use with Iconic, Iconic Styl, Iconic Essence or Pro Series plates. |
Connected Dimmer |