SUG_Wiser_Australia_WSE-04

Blind controllers

Wiser Micro Module Blind

Controls the opening and closing of compatible 240 V AC twin active motorized blinds. Connect up to 10 compatible double momentary push-button switches.

NOTE: Momentary push buttons must be certified for use in 240V AC twin active (4-wire).


Instruction Sheet (PDF)

QR code for this page

Was this helpful?