About the device

The Wiser Window/Door Sensor (hereinafter referred to as sensor) consists of two separate parts: Primary and Secondary. The primary part includes the sensing circuit which detects the secondary part. The secondary part is a magnet.

When the sensor is connected to the Wiser Hub Wiser Gateway and the window/door is opened or closed, the primary part directly reports the change to the app via Wiser Hub Wiser Gateway.

Features of the sensor:

  • Detect when a window or door is open or closed and passes the information to the Wiser Hub.

  • Sends the battery level and offline sensor status information to the Wiser Hub.

Operating elements

  1. Primary part (sensing circuit)

  2. Secondary part (magnet)

  3. Status LED

  4. Function key

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?