Common questions on interconnection setup
Scenarios | Required steps for interconnection | |
---|---|---|
I have only Wiser smoke alarms and Wiser Hub. |
All smoke alarms to be paired to Wiser Hub. |
Follow the steps
in Pairing the device to pair all devices to the same Wiser Hub. |
Only one or part of smoke alarms to be paired to Wiser Hub. |
Test all units to make sure interconnection is correct. Refer testing the interconnected device(s). |
|
I have only Wiser smoke alarms without Wiser Hub. |
Identify one
device as Primary and pair all others according to Interconnecting
devices without Wiser Hub. |
|
I have Wiser smoke alarms and standalone 755LPSMA4 / 755RFB2 smoke alarms / RF base but without Wiser Hub. |
Identify one
device as Primary and pair all others Wiser smoke alarms according
to Interconnecting
devices without Wiser Hub and standalone 755LPSMA4 / 755RFB2
smoke alarms / RF base according to Interconnecting
standalone devices. NOTE: If 755LPSMA4 / 755RFB2 is
already installed and paired before, use the Primary unit to pair
with all Wiser smoke alarms.
|
|
I have Wiser smoke alarms and standalone 755LPSMA4 / 755RFB2 smoke alarms / RF base and Wiser Hub. |
All Wiser smoke alarms to be paired to Wiser Hub. |
Test all units to make sure interconnection is correct. Refer testing the interconnected device(s). NOTE: If 755LPSMA4 / 755RFB2 are already installed
and paired before, reconnect by pairing them again.
|
Only one or part of Wiser smoke alarms to be paired to Wiser Hub. |
Test all units to make sure interconnection is correct. Refer testing the interconnected device(s). NOTE: If 755LPSMA4 / 755RFB2 are already installed
and paired before, reconnect by pairing them again.
|