DUG_Smoke alarm AC Square_CLP-00

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
  • Connecting to installation networks
  • Connecting to several electrical devices
  • Laying electrical cables
  • Safety standards, local wiring rules and regulations
Failure to follow these instructions will result in death or serious injury.
NOTICE
EQUIPMENT INSTALLATION HAZARD
  • Always operate the product in compliance with the specified technical data.
  • Keep the installation instruction for the life of the product.
Failure to follow these instructions can result in equipment damage.
WARNING
SEALED BATTERY HAZARD
Do not recharge, disassemble or incinerate the battery.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?