Getting into a home
-
Register in Wiser app by using an email address or valid mobile number.
See Creating an account. -
Ensure that all the devices are switched on, and the Wiser Hub has Ethernet connection before configuration to complete the commissioning process. After this, configure the device settings.
NOTE: Pairing to other Wi-Fi and BLE enabled devices can also be done during this step. -
Configure the Moments and Automations in the app.
-
Generate the Invitation code/Redeem code and note it on the handover card that is provided in the box/package. Ensure to leave it on the Wiser Hub or in the home.
See Joining a home.
Steps to be performed by the home owner:
-
Register in Wiser app by using an email ID or valid mobile number.
See Creating an account. -
Join a home by providing the invitation code written on the handover card.
-
Power on the Wiser Hub and connect to the Hub by using the router via Ethernet cable. See Ethernet mode connection- Wiser Hub
NOTE: Ethernet cable is provided in the package/box. Hence, it is advised to collect separately and use the cable to connect to the router for better performance. If the home owner needs to Hub using Wi-Fi, see AP mode connection (Wi-Fi)