DUG_Smoke alarm AC Square_CLP-00

Pairing the device

Using the Wiser app , pair your device with the Wiser Hub to access and control the device. You can either add the device manually or do an auto-scan to pair it.
IMPORTANT: Do not mount the device before the pairing. The Setup/Reset button (Zigbee) and power switch are located on the rear side of the device.
NOTE: When multiple smoke alarms are paired with same Wiser Hub , an 433MHz radio frequency (RF) interconnection is automatically created between smoke alarms.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?