Replacing the battery
To replace the battery from the device:
![]() |
---|
CHEMICAL BURN HAZARD
Keep batteries out of reach of children. If swallowed,
seek immediate medical attention.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
NOTICE |
---|
PERFORMANCE DEGRADATION OR EQUIPMENT DAMAGE
• The device should be powered only by the provided
AC adaptor or 4× AA batteries.
• Only alkaline batteries should be used. Do not
use rechargeable batteries.
Failure to follow these instructions can result in equipment damage.
|
-
Rotate the module by 70° clockwise to separate the device from the back cover.
-
Replace the batteries with proper polarity.
-
Position the module to the cover and rotate 70° anti-clockwise.
NOTE: Dispose the used batteries, as per statutory regulations.