DUG_Window/Door Sensor_CLP-00

Installing the device

Refer to the installation instruction supplied with this product.

See Wiser Window/Door Sensor.

NOTICE
EQUIPMENT DAMAGE
  • Do not install the sensor near magnetic devices to avoid degrading its performance.
  • With a window/door in the closed state, the distance between the primary and secondary parts of the sensor should be <18 mm for a non-metallic base (for example, wood or plastic surfaces) and <10 mm for a metallic base.
Failure to follow these instructions can result in equipment damage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.