DUG_Window/Door Sensor_CLP-00

Replacing the batteries

To replace the batteries:
  1. Remove the primary part from the base plate by sliding it upwards.
  2. Unscrew the battery cover using a screwdriver.
    NOTE: The screw is captive, after unscrewing from the primary part it remains attached to the cover.
  3. Replace the battery with the proper polarity.
  4. Re-install the battery cover and tighten the screw using a screwdriver.
    The LED blinks green seven times and then stops blinking.
  5. Install the primary part on the base plate by sliding it down.
    IMPORTANT: Dispose used batteries, as per statutory regulations.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.