DOCA0140EN-03

EcoStruxure Power Commission Software

Overview

EcoStruxure Power Commission software automatically discovers the smart devices and allows you to add the devices for an easy configuration. You can generate comprehensive reports as part of Factory Acceptance Test and Site Acceptance Test to replace your heavy manual work. Additionally, when the panels are under operation, any change of settings made can be easily identified by a yellow highlighter. This indicates the difference between the project and device values, and hence provides a system consistency during the operation and maintenance phase.

EcoStruxure Power Commission software enables the configuration of ComPact NSX circuit breakers with the following modules, and accessories:

  • MicroLogic trip units

  • Communication interface modules: BSCM module, IFM interface, IFE interface, IFE server

  • ULP modules: IO module, FDM121 display

EcoStruxure Power Commission software enables the configuration of the following gateways and wireless devices:

  • EcoStruxure Panel Server

  • PowerTag Link

    gateway
  • PowerTag Energy

    module
  • Wireless indication auxiliary

EcoStruxure Power Commission software is available at www.se.com

Key Features

EcoStruxure Power Commission software performs the following actions for the supported devices and modules:

  • Create projects by device discovery

  • Save the project in the EcoStruxure Power Commission cloud for reference

  • Upload settings to the device and download settings from the device

  • Compare the settings between the project and the device

  • Perform control actions in a secured way

  • Generate and print the device settings report

  • Perform a communication wiring test on the entire project and generate and print test report

  • View the communication architecture between the devices in a graphical representation

  • View the measurements, logs, and maintenance information

  • View the status of device and IO module

  • View the alarm details

  • Check the system firmware compatibility status

  • Update to the latest device firmware

  • Perform force trip and automatic trip curve test

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?