DOCA0140EN-03

Front Face Description

Front Face

A Faceplate

B Toggle handle for opening, closing, and resetting

C Push-to-trip button

D Trip unit setting range

E Trip unit

F Trip unit adjustment dials

For more information about installation, consult the instruction sheets on the Schneider Electric website:

  • GHD16242AA, ComPact NSX 100-250 circuit breakers and switch-disconnectors

  • GHD16243AA, ComPact NSX 400-630 circuit breakers and switch-disconnectors

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?