Locking the Circuit Breaker
Locking Accessories
DANGER |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
When the circuit breaker toggle handle is locked in the
position, always use
a properly rated voltage sensing device to confirm that power is off
before working on equipment.Failure to follow these instructions will result in death or serious injury.
|
Use locking accessories to lock the toggle handle in the I (ON) or O (OFF) position.
Accessory |
Padlocks |
|
---|---|---|
Accessory that is part of the case |
Use up to 3 padlocks (not supplied) 5–8 mm (0.2–0.3 in) in diameter |
|
Accessory that is detachable |
Use up to 3 padlocks (not supplied) 5–8 mm (0.2–0.3 in) in diameter |
Sealing Accessories
Use sealing accessories to prevent circuit breaker operations.
Seal |
Prohibited operations |
|
Escutcheon mounting screw |
|
|
Transparent protective cover |
|
|
Mounting screw for terminal shields |
Accessing the power connection (protection against direct contact) |