Insulated NSX Cord
Introduction
For system voltage greater than 480 Vac, an insulated variant of the NSX cord needs to be used, terminated by an electronic module with a female RJ45 connector. A ULP cord must be used to connect the insulated NSX cord electronic module to a ULP module.
The reference for the insulated NSX cord is LV434204.
The insulated NSX cord electronic module must be supplied with 24 Vdc in order to guarantee isolation of the ULP system.
For more information about installation, consult the instruction sheet on the Schneider Electric website: GHD16313AA ComPact NSX100–630 – Insulated NSX Cord.
Electronic Module Characteristics
The following table summarizes the electronic module characteristics:
Characteristic |
Value |
---|---|
Dimensions |
27 x 27 x 27 mm |
Mounting |
On DIN rail |
Degree of protection of the installed module |
|
Operating temperature |
-25 to +70 °C |
Power supply voltage |
24 Vdc -20%/+10% (19.2–26.4 Vdc) |
Consumption |
|
Insulated NSX Cord Connection
The NSX cord connects to a ULP module:
-
IFM or IFE communication interface
-
FDM121 display
-
IO module
The figure below illustrates the connections from the insulated NSX cord to the Modbus-SL interface for one circuit breaker:
A IFM Modbus-SL interface for one circuit breaker
B RJ45 male/male ULP cable
C Insulated ULP module for system voltage greater than 480 Vac
D Insulated ULP cord for system voltage greater than 480 Vac
E Connector for ComPact NSX circuit breaker internal connection