Commissioning
List of Checks and Inspections
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
When starting up new equipment, or following lengthy downtime, a general check takes just a few minutes. Such a check reduces the risk of a malfunction due to error or oversight.
The following table indicates the checks and inspections to be performed according to the event:
A |
B |
C |
D |
E |
F |
G |
H |
I |
J |
|
---|---|---|---|---|---|---|---|---|---|---|
Before commissioning |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
– |
✔ |
✔ |
✔ |
– |
– |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
|
After carrying out work on the switchboard |
– |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
Periodically during lengthy downtime |
– |
✔ |
– |
✔ |
✔ |
– |
✔ |
– |
✔ |
✔ |
Following lengthy downtime |
– |
✔ |
– |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
Following lengthy downtime and modification to the switchboard |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
✔ |
A Insulation and dielectric strength tests |
A: Insulation and Dielectric Strength Tests
![]() |
---|
HAZARD OF EQUIPMENT DAMAGE
Insulation and dielectric strength tests must only be
carried out by qualified electrical personnel.
Failure to follow these instructions can result in injury or equipment damage.
|
Insulation and dielectric strength tests are carried out before the switchboard is delivered. These tests are subject to the currently applicable standards.
Dielectric strength tests impose great stress on the equipment and can cause damage if performed incorrectly. In particular:
-
Reduce the value used for the test voltage according to the number of consecutive tests on the same piece of equipment
-
Disconnect electronic equipment if necessary
A: Insulation and Dielectric Strength Tests on MicroLogic 4 and 7 Trip Units
NOTICE |
---|
HAZARD OF TRIP UNIT DETERIORATION
Failure to follow these instructions can result in equipment damage.
|
The MicroLogic 4 and 7 trip units have a second power supply (in addition to the power source provided by the current transformers) to power the earth-leakage protection even when the current demand is low. This power supply must be switched off when carrying out dielectric tests.
To switch off this power supply on the MicroLogic 4 trip unit during a dielectric test, follow this procedure.
Step |
Action |
|
---|---|---|
1 |
Remove any seal on the protective cover of the trip unit. |
|
2 |
Open the protective cover of the trip unit by inserting a screwdriver under the clip. |
|
3 |
Push the tip of the screwdriver up to release the clip. |
|
4 |
The cover opens. |
|
5 |
To enable a dielectric test to be carried out, turn the dielectric switch (A) counterclockwise from the vertical position to the Test position (horizontal) by using a flat screwdriver. Result: The switch pops out when the screwdriver is removed. NOTE: Do not close the protective cover during the test.
|
|
6 |
After carrying out a dielectric test, put the switch back to the vertical position: First, push in the switch. |
|
7 |
Keeping the switch pushed in, turn it clockwise from the Test position to the vertical position. Result: The switch stays retracted when the screwdriver is removed. |
|
8 |
Close the protective cover by clipping it back into place. |
|
9 |
Replace the seal. |
|
10 |
After performing the dielectric test, carry out an earth-leakage test. |
– |
![]() |
---|
LOSS OF EARTH-LEAKAGE PROTECTION
The dielectric switch must be in the retracted position
while the circuit breaker is in use.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
A: Insulation and Dielectric Strength Tests on VigiPacT Add-on Devices
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
HAZARD OF EQUIPMENT DAMAGE
Disconnect the protective cover on the front of the VigiPacT Add-on before performing insulation and
dielectric strength tests.
Failure to follow these instructions can result in injury or equipment damage.
|
VigiPacT Add-on and VigiPacT Add-on Alarm are electronic devices which need to be disconnected before dielectric tests. Follow this procedure before carrying out a dielectric test:
Step |
Action |
|
---|---|---|
1 | Before
carrying out a dielectric test, remove any seal from the VigiPacT Add-on mounting screw then unscrew the screws from the protective
cover for the connections (A):
|
|
2 |
Remove the protective cover. NOTE: Removing the protective cover
on the front of the module (A) automatically
disconnects the VigiPacT Add-on.
|
|
3 |
After carrying out a dielectric test, put the protective cover (A) back into place. NOTE: If the protective
cover is not put back:
|
|
4 | Tighten the screws of the protective cover. | |
5 | Replace the seal. | – |
6 | After performing the dielectric test, carry out an earth-leakage test. | – |
A: Dielectric Strength Tests with PowerTag Energy
NOTICE |
---|
hazard of powertag m250/m630 deterioration
Failure to follow these instructions can result in equipment damage.
|
PowerTag Energy is an electronic device which needs to be disconnected before dielectric tests. Follow this procedure before carrying out a dielectric test:
B: Inspect Switchboard
Check that the circuit breakers are installed:
-
In a clean environment without waste from assembling the equipment (such as wiring, tools, shavings, metallic particles)
-
In a properly ventilated switchboard (unobstructed ventilation grills)
C: Check Compliance with the Diagram
Check that the circuit breakers comply with the installation diagram:
-
Identification of the feeds on the front of the circuit breakers
-
Rating and breaking capacity (indications on the faceplate label)
-
Identification of the trip units (type, rating)
-
Presence of additional functions (VigiPacT Add-on earth-leakage protection, motor mechanism, rotary handle, control or indication auxiliaries, locking, sealing)
-
Protection settings (overload, short-circuit, earth-leakage):
-
Thermal-magnetic and MicroLogic 2 and 4 electronic trip units: visually check the position of the adjustment dials
-
MicroLogic 5, 6 and 7 electronic trip units: visually check the position of the adjustment dials for the main settings and use EcoStruxure Power Commission software to check in detail
-
D: Inspect Mechanical Equipment
Visually inspect the general state of the circuit breaker. Check the following items:
-
Terminal shields and interphase barriers
-
Escutcheon
-
Trip unit
-
Case
-
Chassis
Check the equipment integrity: a circuit breaker found with a cracked case or burn marks must be immediately taken out of service and replaced.
Check the mounting and mechanical strength:
-
Of circuit breakers in the switchboard.
-
Of auxiliaries and accessories on the circuit breakers:
-
Rotary handles or motor mechanisms
-
Installation accessories (such as terminal shields and escutcheons)
-
-
Of the chassis (withdrawable circuit breaker)
-
Of locks, padlocks and padlock support tabs
E: Check Connections
Check the tightening torque of the power connections and auxiliary circuit connections, as described in the instruction sheets.
F: Check Mechanical Operation
Check the circuit breaker mechanical operation:
-
Opening, closing and resetting
-
Tripping with the push-to-trip button
-
Tripping by MN/MX control auxiliaries
-
Opening, closing, resetting by motor mechanism in automatic and manual mode
G: Check Electronic Trip Units and VigiPacT Add-on Devices
Check that the following are working correctly:
-
MicroLogic electronic trip units, with the aid of specific maintenance interfaces:
-
Pocket battery
-
Service Interface and a PC running EcoStruxure Power Commission software
-
USB maintenance interface
NOTE: For trip units without test port, check the functions of the trip unit using primary injection. -
-
OF, SD or SDE indication contacts
-
SDx or SDTAM modules
-
VigiPacT Add-on devices and SDV indication contact, by operating the test button T on the front (this test checks the whole measurement system and tripping on earth-leakage faults)
-
Wireless indication auxiliaries
H: Check Pairing of Wireless Devices with Gateway or Panel Server
Check that wireless communication with gateway or Panel Server is working correctly:
-
For PowerTag Energy, LED is blinking green each time data is sent (every 5 seconds by default)
-
For wireless indication auxiliaries, LED is blinking green each time data is sent (every 8 hours, or when status changes).
I: Check Communication
Check that the communication through the communication network works correctly. Refer to DOCA0093EN, ULP System (IEC Standard) – ULP (Universal Logic Plug) System – User Guide.
J: Clean Equipment
To avoid dust deposits that could affect the circuit breaker mechanical operation, clean the circuit breakers when performing maintenance:
-
For non-metallic parts: always use a dry cloth. Do not use cleaning products.
-
For metallic parts: preferably use a dry cloth. If a cleaning product must be used, do not apply or splash the product onto non-metallic parts.